K65 and P&E Debugger connection issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K65 and P&E Debugger connection issue

1,236 Views
anilrayan
Contributor I

I am getting this error while trying to connect to the K65 eval board 

pastedImage_1.png

I see in device manager 

pastedImage_2.png

So PE debugger is detected properly 

Is there any setting i have to do prior using the debugger, Please suggest 

0 Kudos
Reply
1 Reply

1,195 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello ANIL RAYAN,

Please download the newest drivers available for the PE debugger and install them while the debugger is connected to your PC. 

Link to download the drivers

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply