K65 RUNHS mode memset performance is worst than RUN mode.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K65 RUNHS mode memset performance is worst than RUN mode.

1,228 次查看
irfanshahid
Contributor I

Hi,

I am doing some bench-marking on the K65 processor and have seen a strange problem. When the core is run in RUNHS mode (Core = 180MHz, SDRAM = 60MHz, Flash = 25.7MHz), I get ~34MBps performance for memset operation. However, with RUN mode (Core = 120MHz, SDRAM = 60MHz, Flash = 20MHz), I get ~52MBps performance for memset operation.

My code is running is from the Flash and I use external SDRAM for data. Can any body help me understand this strange behavior?

标签 (1)
0 项奖励
回复
1 回复

1,155 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I find the same question at online support system with case number: 00151005

Please check my feedback at case number: 00151005.

Thank you for the understanding.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复