K65 KBOOT 1.2.0 write-memory fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K65 KBOOT 1.2.0 write-memory fails

跳至解决方案
1,429 次查看
ricado
Contributor I

Hi,

I'm using the KBOOT 1.2.0 in a TWR-K65F180M with USB HID and blhost.exe utility, developing  in KDS 3.0 and tower_bootloader project. I changed the default application address in KBOOT bootloader_config.h BL_APP_VECTOR_TABLE_ADDRESS from 0xA000 to 0xB000 because in order to debug the KBOOT it's size is a little bigger than 0xA000 bytes. When I attempt to load my application to the user flash I receive the error 995. It says that 32 bytes were written in flash but I only see the first 8 bytes when I read back the 0xB000 memory. The first 32 bytes sent are:"F8 FF 02 20 D9 B4 00 00 E9 B4 00 00 E9 B4 00 00 E9 B4 00 00 E9 B4 00 00 E9 B4 00 00 00 00 00 00". The memory is erased (all 0xFFs) before I use the write-memory command.

I include the command line input and output.

>>

C:\K65BL>blhost -u 0x15A2,0x0073 get-property 1

Inject command 'get-property'

Response status = 0 (0x0) Success.

Response word 1 = 1258358017 (0x4b010501)

Current Version = K1.5.1

C:\K65BL>blhost -u 0x15A2,0x0073 read-memory 0xb000 32

Inject command 'read-memory'

Successful response to command 'read-memory'

ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff

ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff

Successful generic response to command 'read-memory'

Response status = 0 (0x0) Success.

Response word 1 = 32 (0x20)

Read 32 of 32 bytes.

C:\K65BL>blhost -u 0x15A2,0x0073 write-memory 0xb000 ./myApp.bin

Inject command 'write-memory'

Preparing to send 65048 (0xfe18) bytes to the target.

Successful generic response to command 'write-memory'

GetOverlappedResult failed with error 995: The I/O operation has been aborted because of either a thread exit or an application request.

Data phase write aborted by status 0x1 Failure.

Response status = 10004 (0x2714) No response packet from target device.

Wrote 32 of 65048 bytes.

C:\K65BL>blhost -u 0x15A2,0x0073 read-memory 0xb000 32

Inject command 'read-memory'

Successful response to command 'read-memory'

f8 ff 02 20 d9 b4 00 00 ff ff ff ff ff ff ff ff

ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff

Successful generic response to command 'read-memory'

Response status = 0 (0x0) Success.

Response word 1 = 32 (0x20)

Read 32 of 32 bytes.

<<

Am I missing something in configuration and/or in the blhost commands?

0 项奖励
回复
1 解答
1,178 次查看
ricado
Contributor I

Update SOLVED!!!!

The problem was that the K65 was reseting when attempting to call function "callFlashRunCommand" which runs from RAM and was previously copied. It seems that the RAM memory allocated to copy the function was smaller than the function's size, the calculation might have been done once the bootloader was fully optimized but I don't think allocating more space does any harm.

So I changed

enum _flash_execute_in_ram_function_constants

{

--     kFlashExecuteInRamFunction_MaxSize   = 32,

++   kFlashExecuteInRamFunction_MaxSize   = 64,

       kFlashExecuteInRamFunction_TotalNum  = 2

};

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,179 次查看
ricado
Contributor I

Update SOLVED!!!!

The problem was that the K65 was reseting when attempting to call function "callFlashRunCommand" which runs from RAM and was previously copied. It seems that the RAM memory allocated to copy the function was smaller than the function's size, the calculation might have been done once the bootloader was fully optimized but I don't think allocating more space does any harm.

So I changed

enum _flash_execute_in_ram_function_constants

{

--     kFlashExecuteInRamFunction_MaxSize   = 32,

++   kFlashExecuteInRamFunction_MaxSize   = 64,

       kFlashExecuteInRamFunction_TotalNum  = 2

};

0 项奖励
回复