K65 Allowing for Cache and DMA coherence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K65 Allowing for Cache and DMA coherence

2,264 Views
unknowncoder
Contributor III

Background

  • I am looking at enabling the code cache controller on the K65 to improve performance.
  • I utilize DMA for peripheral to memory and memory to peripheral transfer.
  • I know cache and DMA don't normally work good together and the normal operation is to invalidate the cache before/after, read/write respectively.

Question

  • From the Table 30-1 it shows that SRAM is non-cacheable. Given this if I make sure that all access with DMA occurs within SRAM would I need to invalidate the cache still?

Thanks

Labels (1)
Tags (4)
0 Kudos
Reply
3 Replies

2,192 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, you are right. SRAM in K65 is a kind of TCM. Its speed is same as M4 kernel. It needn't cache.

Regards,

Jing

0 Kudos
Reply

2,192 Views
unknowncoder
Contributor III

Are both upper and lower memory tightly coupled memory to the core? 

0 Kudos
Reply

2,192 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes.

Regards,

Jing

0 Kudos
Reply