K64F VLPS Current Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K64F VLPS Current Problem

2,336 次查看
parkjaichang
Contributor I

Hi I'm using the Hexiwear (K64F Family) and MCUXpresso IDE.

My Debugger is Hexiwear Docking Station.

I tried to VLPS mode from VLPR. But VLPS current is to High.(About 9 - 10mA measured a whole board)

First. I Copied and pasted Reference Code a.

Second. Fixed Clock Frequency(Used MCUXpresso Config Tool) and LLWU pin ( changed PTC6 to PTA4 ( LLWU_P3) )

Then, Debugging and measurement current value.

  • I attached Two zip file of My code.
  1. 1. Hexi_Project.zip : power_manager code
  2. 2. MK64FN1M0xxx12_Project : power_mode_switch code

  • Questions
  1. How to Fix this problem.? 
  2. I read AN4503 2.3.9 VLPS (page11) but How to set debugger disable in MCUXpresso IDE?

Thanks

Jeffrey.

  • Reference Code.
  1. 1. SDK_2.3.1_FRDM-K64F\boards\frdmk64f\demo_apps\power_manager
  2. 2. SDK_2.3.1_FRDM-K64F\boards\frdmk64f\demo_apps\power_mode_switch
  3. 3. AN4503 : Power management for Kinetis MCUs.
  4. 4. An4470 :Using Low Power modes on Kinetis Family
标签 (1)
标记 (5)
0 项奖励
回复
3 回复数

2,167 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please remove the debugger tool, then let the application running from internal Flash and measure the power consumption at VLPS mode.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,167 次查看
parkjaichang
Contributor I

How to remove the debugger tool? and How to Set the application running from internal Flash?

Can I get some References and method??

Thanks 

0 项奖励
回复

2,167 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

The SDK V2.3.1 [power_manager] or [power_mode_switch] demo default running from internal Flash.

During project debug phase(through DEBUG panel), the demo was programmed to K64 internal Flash.

After that, customer can power off the K64 board and remove the debugger tool, then power on K64 board and the demo will run from internal Flash.

From the serial console, customer can select the VLPS low power mode and measure the power consumption.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复