K64F, GDB load failed after RAM relocating (solved)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64F, GDB load failed after RAM relocating (solved)

2,717件の閲覧回数
Onemars
Contributor II

Hello,

I'm working with a MK64FN1M0VLL12 in Kinetis Design Studio 3.2.0, I have a const buffer of 64 bytes allocated at 0x000F F000 and a RAM buffer of 64 bytes allocated at 0x2000 0000.

I've tried to follow "Relocating Code and Data Using the KDS GCC Linker File for Kinetis".

I can compile without errors but I cannot debug because I get the error "CMSIS-DAP: Write Error (0x04)" after "writing buffer of 64 byte at 0x000ff000".

But if I don't force the location of one of the two buffers, so the const buffer goes in the m_text section, or the RAM buffer goes in the m_data section, it works.

Do you know what it is wrong with this relocation?

Thank you,

Gabriele


This is the code:

#include "board.h"
#include "pin_mux.h"
#include "clock_config.h"

__attribute__ ((section(".xxx")))
uint8_t ucHeap[64];

__attribute__ ((section(".params")))
const uint8_t pars[64];

int main(void)
{
    BOARD_InitPins();
    BOARD_BootClockRUN();

    memset(ucHeap, 0xEE, sizeof(ucHeap));
    memcpy(ucHeap, pars, sizeof(pars));

    for (;;)
        __asm("NOP");
}

These are the changes done on the linker file:

MEMORY
{
  m_interrupts          (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00000400
  m_flash_config        (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000010
  m_text                (RX)  : ORIGIN = 0x00000410, LENGTH = 0x000FEBF0
  m_params              (RW)  : ORIGIN = 0x000FF000, LENGTH = 0x00000100
  m_data                (RW)  : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
  m_data_2              (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00030000
}

... (after .text)
  .params_section :
  {
    . = ALIGN(4);
    KEEP (*(.params))
    . = ALIGN(4);
  } > m_params

... (after .bss)
  .xxx_section : 
  {
    *(.xxx)
  } > m_data_2

And this is the error:

Debug: 457 821 gdb_server.c:2647 gdb_input_inner(): received packet: 'Xff000,40:<binary-data>'
Debug: 458 821 gdb_server.c:1495 gdb_write_memory_binary_packet(): addr: 0x000ff000, len: 0x00000040
Debug: 459 821 target.c:1849 target_write_buffer(): writing buffer of 64 byte at 0x000ff000
Error: 460 832 cmsis_dap_usb.c:489 cmsis_dap_swd_write_reg(): CMSIS-DAP: Write Error (0x04)
Error: 461 836 arm_adi_v5.c:363 mem_ap_write(): Failed to write memory at 0x000ff004
Debug: 462 836 gdb_server.c:2647 gdb_input_inner(): received packet: 'X20000000,40:<binary-data>'
Debug: 463 836 gdb_server.c:1320 gdb_error(): Reporting -4 to GDB as generic error
Debug: 464 836 gdb_server.c:1495 gdb_write_memory_binary_packet(): addr: 0x20000000, len: 0x00000040
Debug: 465 836 target.c:1849 target_write_buffer(): writing buffer of 64 byte at 0x20000000
Debug: 466 871 gdb_server.c:2649 gdb_input_inner(): received packet: 'qL1200000000000000000'
Debug: 467 871 gdb_server.c:2649 gdb_input_inner(): received packet: 'm4d8,4'
Debug: 468 872 gdb_server.c:1363 gdb_read_memory_packet(): addr: 0x000004d8, len: 0x00000004
Debug: 469 872 target.c:1910 target_read_buffer(): reading buffer of 4 byte at 0x000004d8
Debug: 470 878 gdb_server.c:2649 gdb_input_inner(): received packet: 'D'
Debug: 471 878 target.c:1395 target_call_event_callbacks(): target event 24 (gdb-detach)
Debug: 472 878 gdb_server.c:1002 gdb_connection_closed(): GDB Close, Target: kinetis.cpu, state: halted, gdb_actual_connections=0
Debug: 473 878 target.c:1395 target_call_event_callbacks(): target event 6 (gdb-end)
Debug: 474 878 target.c:1395 target_call_event_callbacks(): target event 24 (gdb-detach)
Info : 475 878 server.c:476 server_loop(): dropped 'gdb' connection

And the GDB trace:

924,536 &"load F:\\\\PROGETTI\\\\Workspace\\\\test_ram\\\\Debug\\\\test_ram.elf\n"
924,537 ~"Loading section .params_section, size 0x40 lma 0xff000\n"
924,537 25+download,{section=".params_section",section-size="64",total-size="663166"}
924,537 25+download,{section=".params_section",section-sent="64",section-size="64",total-sent="64",t\
otal-size="663166"}
924,537 ~"Loading section .xxx_section, size 0x40 lma 0x20000000\n"
924,552 &"Load failed\n"
924,552 25^error,msg="Load failed"
924,553 (gdb)
924,554 27-gdb-exit
924,593 26^done,threads=[{id="1",target-id="Remote target",frame={level="0",addr="0x000004d8",func="\
Reset_Handler",args=[],file="../startup/startup_MK64F12.S",fullname="F:\\PROGETTI\\Workspace\\test_r\
am\\startup\\startup_MK64F12.S",line="326"},state="stopped"}]
924,593 (gdb)
924,594 27^exit
924,594 =thread-group-exited,id="i1"

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,386件の閲覧回数
Onemars
Contributor II

As described here, it is possible that the kinetis driver of OpenOCD is not able to automatically recognizes the second flash bank. By manually configuring both the banks of the MK64FN1M0VLL12 I was able to solve the problem.

0 件の賞賛
返信

2,386件の閲覧回数
Onemars
Contributor II

A clumsy workaround is to define the RAM buffer as 'extern' and then define its address in the SECTIONS of the linker file:

ucHeap = 0x20000000;

It is necessary to manually allocate the buffer by moving the start of m_data_2 in the MEMORY section:

m_data_2              (RW)  : ORIGIN = 0x20000100, LENGTH = 0x0002FF00
0 件の賞賛
返信