K64 based USB device using I2S Codec, reasonable?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K64 based USB device using I2S Codec, reasonable?

跳至解决方案
2,184 次查看
EdSutter
Senior Contributor II

I'm working on something that will eventually look like a USB-audio device

(multiple channels in and out).  I have a codec and AFE designed, now I need

to pick a microcontroller with I2S/I2C interfaces hooked to the codec, and then

have either Ethernet or USB as the backend connection to a host.

Ethernet is not a problem; however, I don't have much experience with USB

coding  (point being: I'm hoping the stack does most of the work for me).

Is the K64 a reasonable place to start for a project like this?

Any pointers regarding USB audio would be a help as well...

Thanks in advance,

Ed

标记 (1)
0 项奖励
回复
1 解答
1,902 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Ed,

I think the K64 can meet all your requirements and it's brilliant to choose K64 to start.

SDK shares USB audio demos which integrates with the K64 and please go to download the most updated version through the link as below.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS-SDK&nodeId=0152101E8C1EF7&uc=...

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,903 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Ed,

I think the K64 can meet all your requirements and it's brilliant to choose K64 to start.

SDK shares USB audio demos which integrates with the K64 and please go to download the most updated version through the link as below.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KINETIS-SDK&nodeId=0152101E8C1EF7&uc=...

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,902 次查看
EdSutter
Senior Contributor II

Thanks, i'll give this a shot, and report my results...

0 项奖励
回复