K64 UART TX/RX pin Reassignment?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K64 UART TX/RX pin Reassignment?

跳至解决方案
3,702 次查看
johnbaker
Contributor IV

I have been tasked with using pins PTA16 and PTA17 for RX and TX to a UART (any UART) on the K64.  Based on what I can research so far I do not think it is possible.  Am I wrong?

Thanks,

John Baker

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,470 次查看
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,471 次查看
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

0 项奖励
回复
3,470 次查看
johnbaker
Contributor IV

That’s what I thought. I just wanted to make sure I was not missing anything. We are using PTA14 and 15 now with UART0 so we should be good.

Thanks!!

John

0 项奖励
回复