K64 UART TX/RX pin Reassignment?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 UART TX/RX pin Reassignment?

Jump to solution
3,558 Views
johnbaker
Contributor IV

I have been tasked with using pins PTA16 and PTA17 for RX and TX to a UART (any UART) on the K64.  Based on what I can research so far I do not think it is possible.  Am I wrong?

Thanks,

John Baker

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,326 Views
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

View solution in original post

0 Kudos
Reply
2 Replies
3,327 Views
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

0 Kudos
Reply
3,326 Views
johnbaker
Contributor IV

That’s what I thought. I just wanted to make sure I was not missing anything. We are using PTA14 and 15 now with UART0 so we should be good.

Thanks!!

John

0 Kudos
Reply