K64 UART TX/RX pin Reassignment?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 UART TX/RX pin Reassignment?

ソリューションへジャンプ
3,705件の閲覧回数
johnbaker
Contributor IV

I have been tasked with using pins PTA16 and PTA17 for RX and TX to a UART (any UART) on the K64.  Based on what I can research so far I do not think it is possible.  Am I wrong?

Thanks,

John Baker

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,473件の閲覧回数
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,474件の閲覧回数
mjbcswitzerland
Specialist V

John

These pisn don't have UART Tx/Rx functionality.

The closest they coulld do is UART0_CTS_b and UART0_RTS_b.

Regards

Mark

0 件の賞賛
返信
3,473件の閲覧回数
johnbaker
Contributor IV

That’s what I thought. I just wanted to make sure I was not missing anything. We are using PTA14 and 15 now with UART0 so we should be good.

Thanks!!

John

0 件の賞賛
返信