K64 Signal Multiplexing & Pin Assignments Table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 Signal Multiplexing & Pin Assignments Table

2,625 Views
jtrepanier
Contributor I

Does the K64 Signal Multiplexing & Pin Assignments Table exist someplace in an Excel format that I can use in my design documentation without having to recreate it?

0 Kudos
Reply
3 Replies

2,288 Views
mjbcswitzerland
Specialist V

Hi

I was expecting that someone would have created such a document, but in case it turns out that no one has I have attached the K60 (with K64) port simulation file from the uTasker project which contains the pinout and functions in an array - not exactly EXCEL but almost comma seperated so may be easier to embed if needed.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K64: http://www.utasker.com/kinetis/FRDM-K64F.html / http://www.utasker.com/kinetis/TWR-K64F120M.html / http://www.utasker.com/kinetis/TWR-K65F180M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

:smileyinfo: Out-of-the-box support for 46 Kinetis boards and 10 IDEs (460 combinations from a single code source with no porting required)

0 Kudos
Reply

2,288 Views
jtrepanier
Contributor I

Thanks Mark - I can work with that and it will save me a lot of typing!

Jerry

0 Kudos
Reply

2,288 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Jerry Trepanier,

      We don't have the excel format, we just have the table in the reference manual and datasheet, if you want to use it in your own document, you need to refer to the reference manual(chapter 10.3.1 K64 Signal Multiplexing and Pin Assignments) and recreate it by yourself.

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply