K64 Maximum Sustained Ethernet Data Rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 Maximum Sustained Ethernet Data Rate

1,951件の閲覧回数
marks
Contributor IV

What is the maxim sustained data rate on the Ethernet interface on the K64? Is there example code available to demonstrate this on the K64 Freedom Board?

0 件の賞賛
返信
2 返答(返信)

1,786件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please have a look at FNET [bench] example for FRDM-K64F board about Ethernet throughput.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,786件の閲覧回数
mjbcswitzerland
Specialist V

Hi Mark

You will need to be more precise as to the protocol to be used to get meaningful values.
For example, if you are sending jumbo frames you will easily achieve 100Mb/s but if you are using TCP it will be very much dependent on the stack used and the buffer sizes available and allocated. UDP will give higher sustained throughput due to lower SW overhead and not buffering requirements.
Also the network activity will also be a factor in a real system which may reduce the throughput at no fault of the K64.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
Kinetis K64:
- http://www.utasker.com/kinetis/FRDM-K64F.html
- http://www.utasker.com/kinetis/TWR-K64F120M.html
- http://www.utasker.com/kinetis/TEENSY_3.5.html
- http://www.utasker.com/kinetis/Hexiwear-K64F.html


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 件の賞賛
返信