K64 Factory Programmed Firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 Factory Programmed Firmware

1,592件の閲覧回数
ramstell
Contributor III

We are currently developing using a TWR-K64F-120M Tower Module with a view to use a K64 processor in our own board.

Can you confirm what firmware, if any, is pre-programmed into the device from the factory?

In the Kinetis Bootloader Manual it states the following:

All future Kinetis devices will arrive with a ROM containing the Kinetis bootloader, while others will arrive pre-programmed from the factory with a one-time-use serial flashloader.

Reading the forum and applications notes, however, do not mention that this is the case. Calcification would be much appreciated.

Kind regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,463件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Roger Amstell:

The K64 does not have the flashloader integrated from factory. Please check the table in next product page for the supported devices in each category (flash-resident bootloader/flashloader/ROM bootloader):

Kinetis Bootloader|Freescale

From the same link you can download the bootloader firmware to use it with the K64.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信