K64 Factory Programmed Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 Factory Programmed Firmware

1,582 Views
ramstell
Contributor III

We are currently developing using a TWR-K64F-120M Tower Module with a view to use a K64 processor in our own board.

Can you confirm what firmware, if any, is pre-programmed into the device from the factory?

In the Kinetis Bootloader Manual it states the following:

All future Kinetis devices will arrive with a ROM containing the Kinetis bootloader, while others will arrive pre-programmed from the factory with a one-time-use serial flashloader.

Reading the forum and applications notes, however, do not mention that this is the case. Calcification would be much appreciated.

Kind regards

Labels (1)
0 Kudos
Reply
1 Reply

1,453 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Roger Amstell:

The K64 does not have the flashloader integrated from factory. Please check the table in next product page for the supported devices in each category (flash-resident bootloader/flashloader/ROM bootloader):

Kinetis Bootloader|Freescale

From the same link you can download the bootloader firmware to use it with the K64.

I hope this clarifies.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply