K64 FTFE Write Lower and Upper 32-bits in Seperate Commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K64 FTFE Write Lower and Upper 32-bits in Seperate Commands

963件の閲覧回数
Mike_d
Contributor IV

I want to write the internal flash 32-bits at a time as I was able to do with FTFL.

The FTFE apparently writes 64-bits at a time (instructions are 32-bits right?) so I'm writing the lower 32-bits with the upper set to 0xFFFFFFFF.

I then follow it up with another write where the lower 32-bits is the same and the upper 32-bits has new data.

Strange things happen when I do this and MGSTAT0 gets set.  Any ideas?

ラベル(1)
0 件の賞賛
返信
1 返信

802件の閲覧回数
mjbcswitzerland
Specialist V

Michael

The K64F uses phrase programming (64 bit word) and it is not possible to program long words.

If you write to a single phrase twice, without erasing the sector that it is in, it can cause a serious flash error (the flash line may become unreadable without erasing it again) and therefore you must avoid writing like this.

As the data sheet specifies, mutliple writes are illegal, so there is no option but to modify the usage of the memory accordingly.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

K64: http://www.utasker.com/kinetis/FRDM-K64F.html / http://www.utasker.com/kinetis/TWR-K64F120M.html / http://www.utasker.com/kinetis/TWR-K65F180M.html

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信