K64 FRDM Board CAN demo working example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64 FRDM Board CAN demo working example

1,319 Views
abhees
Contributor I

Hi,

I,m using K64 Frdm board and i want to test the CAN protocol working.

Is there any working code demo for the CAN project ?

I'm using KDS 3.0 and KSDK1.3.0.

Please help in this.

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

1,171 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Abhinand V

You can find a working example code of CAN in SDK v2.x, you can download the software in the link:

Welcome | MCUXpresso SDK Builder 

The example is located in the path: SDK_2.3.0_FRDM-K64F/boards\frdmk64f\driver_examples\flexcan

Hope this information helps

Best regards

0 Kudos
Reply