K61 MPU User Mode Access Control bit assignments

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K61 MPU User Mode Access Control bit assignments

1,667件の閲覧回数
isaotakashima
Contributor IV

I would like to implement MPU function. The MPU_RGDn_WORD2 registers has 4 User Mode Access Control fields (M3UM, M2UM, M1UM, M0UM).

These fields enable read (r), write (w), and execute ( x) permissions.

I want to make sure that which bit assign read (r), write (w), and execute ( x) permissions.

Regarding the M3UM, this field assigned bit 20, 19 and 18 of MPU_RGDn_WORD2.

I believe that read (r), write (w), and execute ( x) assigned as below:

- bit 20: read (r)

- bit 19: write (w)

- bit 18: execute ( x)

Am I correct?

Please reply as soon as possible.

Best regards,

Takashima

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,545件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hello Takashima,

you are right.

Best regards,

Yasuhiko Koumoto.

0 件の賞賛
返信