K61 FLEXCAN has no DMA support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K61 FLEXCAN has no DMA support

Jump to solution
2,303 Views
benjaminschroed
Contributor III

I've been looking at the Kinetis K series processors, and it appears the CAN interface (FLEXCAN) has no DMA support, only interrupt.  Is this correct, or is there a workaround to be able to utilize DMA, specifically for Rx?

Thanks.

Tags (2)
0 Kudos
Reply
1 Solution
2,072 Views
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

View solution in original post

0 Kudos
Reply
2 Replies
2,073 Views
miduo
NXP Employee
NXP Employee

Hi,

Yes, you are correct. For Kinetis K61, FlexCAN is not a DMA request source and there has no way to use like that.

0 Kudos
Reply
2,072 Views
benjaminschroed
Contributor III

Thank you for the confirmation.

0 Kudos
Reply