K61 Controller Ethernet Link problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K61 Controller Ethernet Link problem

ソリューションへジャンプ
2,346件の閲覧回数
mani8421
Contributor II

We are working with KSZ8041NL for our requirement with K61 Controller.

 

when we are connecting the Ethernet cable to the Jack the two status LED’s simultaneously go ON and OFF continuously as long it is connected. And the link is not established between Host PC.


Can any suggest what could be the problem

ラベル(1)
0 件の賞賛
返信
1 解決策
2,257件の閲覧回数
mani8421
Contributor II

hello Mark,

        Thanks for the Reply.

   we have shorted out the problem. the problem was because of the jack. once when we replaced the jack it worked.

Thanks and regards,

     MANI

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,258件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The LEDs connected to the KS8041NL are controlled by the KS8041NL itself and not the Kinetis. Check the strap inputs which define the meaning of the LEDs - blinking LEDs usually means that there is activity but in your case it sounds that they may not be working in defined modes (there are some reserved modes that should be avoided). Generally check all strap inputs because strapping to an incorrect mode may also cause unexpected behaviour.

Check that your SW can communicate with the KS8041NL via the management port and check also the register settings to ensure that it is not, for example, strapping to isolation mode (or similar.

Regards

Mark

2,258件の閲覧回数
mani8421
Contributor II

hello Mark,

        Thanks for the Reply.

   we have shorted out the problem. the problem was because of the jack. once when we replaced the jack it worked.

Thanks and regards,

     MANI

0 件の賞賛
返信