K60fx512 flex memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60fx512 flex memory

4,230 Views
kristies1
Contributor II

on K60fx512 when I try to partition flex memory, the code hangs (in debugger) or mcu resets where shown below.  Code is based on flexmem_demo.

If I put breakpoint at the hang location and then reset, the flexmem has actually partitioned and works as expected as an eeprom.

Also using MQX 3.8/Codewarrior 10.2 , if this is relevant.

#define DFLASH_SIZE_448   0x04

#define EEPROM_512_512 0x34   // subsystem A = 512 bytes, subsystem B = 512 bytes

void  flexinit (void)

{

        SCB_SHCSR|=SCB_SHCSR_BUSFAULTENA_MASK|SCB_SHCSR_MEMFAULTENA_MASK|SCB_SHCSR_USGFAULTENA_MASK;

        /* Partition the memory to enable FlexMem mode */

        if ( partition_flash( EEPROM_512_512, DFLASH_SIZE_448) )

        {

            /* Wait for the command to complete */

            while(!(FTFE_FCNFG & FTFE_FCNFG_EEERDY_MASK))

            {

            }

        }

}

int partition_flash(int eeprom_size, int dflash_size)

{

   /* Test to make sure the device is not already partitioned. If it

       * is already partitioned, then return with no action performed.

       */

      if ((SIM_FCFG1 & SIM_FCFG1_DEPART(0xF)) != 0x00000F00)

      {

          printf("\nDevice is already partitioned.\n");

          return 0;

      }

    

      /* Write the FCCOB registers */

      FTFE_FCCOB0 = FTFE_FCCOB0_CCOBn(0x80); // Selects the PGMPART command

      FTFE_FCCOB1 = 0x00;

      FTFE_FCCOB2 = 0x00;

      FTFE_FCCOB3 = 0x00;

      /* FCCOB4 is written with the code for the subsystem sizes (eeprom_size define) */

      FTFE_FCCOB4 = eeprom_size;

      /* FFCOB5 is written with the code for the Dflash size (dflash_size define) */

      FTFE_FCCOB5 = dflash_size;

      /* All required FCCOBx registers are written, so launch the command */

      FTFE_FSTAT = FTFE_FSTAT_CCIF_MASK;

      /* Wait for the command to complete */

      while(!(FTFE_FSTAT & FTFE_FSTAT_CCIF_MASK))

      {

// hangs or resets here

      }

      return 1;

}


0 Kudos
Reply
4 Replies

3,492 Views
deekay
Contributor I

Hi

I am also struggling with the flexNVM.

Do you have any core optimization enabled? I.e. -O compile flag?

I have managed to "destroy" a K10DX device when trying to block erase the flash from code, to be able to repartition the memory. I am not sure why it happen, but I think it is because an errata issue, or I did something very wrong....

I ran into an other problem when trying to write to an already partitioned EEEPROM, but I got a hard_fault problem when writing to other flexRAM address than 0x1400 0000. Do not know why. Something you have experienced?

BR

Daniel

0 Kudos
Reply

3,492 Views
kristies1
Contributor II

I had to add the code

     asm("cpsid.n i");          //disable interrupts

before the first FCCOB  write

and the enable interrupts

     asm("cpsie.n i  ");     // enable interrupts

after the wait  for the commands to complete.

This fixed the  lock-up problems with MQX.

I use optimization level 1, and do not try block erase from code.  I have no seen any problems in the flexRAM, and use addresses  past 0x14000200.  But depending on how its partitioned, you may get the hard_fault if you used flexRAM address outside the partitioned area.

0 Kudos
Reply

3,492 Views
deekay
Contributor I

Ok. Perhaps the partitioning went bad due to lack of interrupt disabling. That might explain why I couldn't access addresses > 0x1400 0000 without hard_fault.

Yes I did use the block erase command from inside code... That seems to have corrupted the flash so I cannot program in via JTAG anymore. As according to errata e3854 described in KINETIS_0M33Z.pdf.I guess I shall use Erase Flash Sector command instead to prepare flexNVM for re-partitioning, have you tried it?


Do you know any workarounds to make it "come back from the dead"? Or shall I consider it scrap....


BR

Daniel

0 Kudos
Reply

3,492 Views
kristies1
Contributor II

The dflash always gets erased by codewarrior, so I don't have to worry about erasing prior to partitioning.  According to the datasheets, the app should only partition once for the lifetime of the device.

0 Kudos
Reply