K60N512 running QNX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60N512 running QNX

Jump to solution
1,486 Views
descor
Contributor I

Hello All,

I am interested in using the K60N512 MCU board. I was wondering if freeScale provides a board support package that has QNX?

Regards

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,307 Views
DavidS
NXP Employee
NXP Employee

To add to Kan reply.  QNX has much support for Freescale processors with MMU's.  Kinetis devices do not have MMU and therefore no QNX support.

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
1,308 Views
DavidS
NXP Employee
NXP Employee

To add to Kan reply.  QNX has much support for Freescale processors with MMU's.  Kinetis devices do not have MMU and therefore no QNX support.

Regards,

David

0 Kudos
Reply
1,307 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Des Cor,

So far, QNX is not supported by KSDK, while MQX, FreeRTOS and UCOS are supported, and we have a new sub space for KSDK now, you may refer to https://community.freescale.com/community/kinetis/kinetis-software-development-kit for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply