K60N512 running QNX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,156件の閲覧回数
descor
Contributor I

Hello All,

I am interested in using the K60N512 MCU board. I was wondering if freeScale provides a board support package that has QNX?

Regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,977件の閲覧回数
DavidS
NXP Employee
NXP Employee

To add to Kan reply.  QNX has much support for Freescale processors with MMU's.  Kinetis devices do not have MMU and therefore no QNX support.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,978件の閲覧回数
DavidS
NXP Employee
NXP Employee

To add to Kan reply.  QNX has much support for Freescale processors with MMU's.  Kinetis devices do not have MMU and therefore no QNX support.

Regards,

David

0 件の賞賛
返信
1,977件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Des Cor,

So far, QNX is not supported by KSDK, while MQX, FreeRTOS and UCOS are supported, and we have a new sub space for KSDK now, you may refer to https://community.freescale.com/community/kinetis/kinetis-software-development-kit for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信