K60 s19 file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 s19 file

1,137件の閲覧回数
miroslavtovilov
Contributor I

How I can make a SAP file for CYCLONE MAX.

First I set up Eclipse to create flash image , and I got file .hex

Cyclone ImageCreation.png

I try and make it, but when I program K60 I have a error  00000007.

What is wrong ? MAX_error.jpg

ラベル(2)
0 件の賞賛
返信
1 返信

993件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I checked the Cyclone MAX user manual, the $0007 error(Error entering debug mode) belongs to  debug mode communication error.

Please check the K60 board debugger circuit if it works.

Customer could refer KQRUG file chapter 2.1.5.3 about K60 debug interface.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信