K60 flexNVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 flexNVM

Jump to solution
2,980 Views
bryano
Contributor II

I am having an issue running the "flexmem" demo.  I am unclear why it hangs where indicated below.

 

Here are the details:

 

* K60 Tower board (TWR-K60N512).  It has mask 0M33Z silicon.  The only errata that appears to pertain is errata ID 2592.  However, the example code takes that into account.

 

* Using IAR tools (ver 6.4).  It uses the same flexmem demo that come with CodeWarrior 10.2 (Freescale\CW MCU 10.2\MCU\CodeWarrior Examples\K40\flexmem)   There isn't a flexmem example in the K60 directory.

 

void main (void)
{
    char ch;
        uint32 timeout;
                 SCB_SHCSR|=SCB_SHCSR_BUSFAULTENA_MASK|SCB_SHCSR_MEMFAULTENA_MASK|SCB_SHCSR_USGFAULTENA_MASK;
      printf("\nRunning FlexMem demo!!\n");

        /* Partition the memory to enable FlexMem mode */
        if ( partition_flash( EEPROM_16_16, DFLASH_SIZE_128) )
        {
            /* Device has been partitioned for the first time, so this
             * means the counters have not been initialized yet. We'll
             * zero them out now.
             */
            *((uint32 *)(LONGWORD_COUNTER_ADDR)) = 0x0;

            /* Wait for the command to complete */
            while(!(FTFL_FCNFG & FTFL_FCNFG_EEERDY_MASK));  <<<<<hangs here

0 Kudos
Reply
1 Solution
2,225 Views
ndavies
Contributor V

The K60 MCU on the TWR-K60N512 doesn't have any NVM. It's a flash only part. The N in the K60 part number signifies a flash only part. You would need an X in that position to signify a part with NVM.

View solution in original post

0 Kudos
Reply
2 Replies
2,226 Views
ndavies
Contributor V

The K60 MCU on the TWR-K60N512 doesn't have any NVM. It's a flash only part. The N in the K60 part number signifies a flash only part. You would need an X in that position to signify a part with NVM.

0 Kudos
Reply
2,225 Views
bryano
Contributor II

Thanks.  I discovered that fact after already posting.

0 Kudos
Reply