K60 USB device code not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 USB device code not working

2,460件の閲覧回数
Ruds
Contributor I

Hi all,

I have downloaded the USB device  code provided by freescale developers to my Cortex M4 K60 board where i have not used any external pullups and MAX3353EEUE IC for the circuit,

i made few changes in the code, those are

 

1.  Disabled weak pull downs ==> USB0_USBCTRL &= ~0x40;(Because DP line was detecting its Voltage up to +1.2V only) in USB.C

2. sellected Clock source as FLL insted of PLL in USB.H

3.defined NO_PLL_INIT = 1 in sysinit.C

 

my problems are

1.after running the program its contineously displays "Enter USB Reset handler"

 

 

please help me to solve this problem....

Thank you so much

0 件の賞賛
返信
1 返信

2,073件の閲覧回数
bugs
Contributor III

We never get the USB working with FLL. you'd better use PEE mode.

Even don't try to use internal clock for UART, the baudrate difference is too big.

0 件の賞賛
返信