K60 UART Pullup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 UART Pullup

1,869 Views
johnaraujo
Contributor I

We are using the K60FN1M0VLQ12. I want to use the internal pullups on UART4_RX (pin 119) and UART2_RX  (pin 129). Will the pullups remain enable even when we configure these pins for the UART ALT3 functions? Thank!

0 Kudos
Reply
1 Reply

1,786 Views
mjbcswitzerland
Specialist V

Hi John

Yes, pull-ups are valid for the UART input functions.

In the uTasker project it is done with

_CONFIG_PERIPHERAL(D, 2, (PD_2_UART2_RX | UART_PULL_UPS));   // UART2_RX on PD2 (alt. function 3)

and
_CONFIG_PERIPHERAL(C, 14, (PC_14_UART4_RX | UART_PULL_UPS)); // UART4_RX on PC14 (alt. function 3)

Otherwise you just need to set the PORTD_PCR2 and PORTC_PCR14 registers to have their ALT fields set to 3 and their pulls polarity and enable to 0x03.

Pull-ups on the UART inputs ensures that they don't float in low power modes, which can otherwise cause higher than expected current consumption.

Regards

Mark


Complete K60 solutions, training and support:http://www.utasker.com/kinetis.html
Kinetis K60:
- http://www.utasker.com/kinetis/TWR-K60N512.html
- http://www.utasker.com/kinetis/TWR-K60D100M.html
- http://www.utasker.com/kinetis/TWR-K60F120M.html
- http://www.utasker.com/kinetis/ELZET80_NET-KBED.html
- http://www.utasker.com/kinetis/ELZET80_NET-K60.html

0 Kudos
Reply