K60 Tower MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 Tower MQX

3,060件の閲覧回数
manu_00
Contributor II

Hi,

did anyone get the AN3905 (Writing your first MQX Application) runing on the TWR-K60N512?

I tried it but i am strugeling with the defines for the LEDs in ioDriver.c

#define LED_1 (GPIO_PORT_TE | GPIO_PIN3)

i thought i can change this statement to

#define LED_1 (GPIO_PIN11).....  GPIO_PIN11 is the Pin on wich LED1 is connected.

but it doesn't work. Is there anything else i have to llok for?

Thanks

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,694件の閲覧回数
carlos_neri
NXP Employee
NXP Employee

manu,

You can try with the following:

#define LED1                    (GPIO_PORT_A | GPIO_PIN11)

#define LED2                    (GPIO_PORT_A | GPIO_PIN28)

#define LED3                    (GPIO_PORT_A | GPIO_PIN29)

#define LED4                    (GPIO_PORT_A | GPIO_PIN10)

Note that you need to specify the port, in this case, port A and the pin.

Also MQX already has these definitions. If you're interested in using them, these are:

BSP_LED1  

BSP_LED2  

BSP_LED3  

BSP_LED4  

You can find them on the "twrk60n512.h" file at:

{MQX path}\lib\twrk60n512.cw10\bsp

Note that the specific BSP folder may change if you're using a different toolchain (IAR or Keil)

2,694件の閲覧回数
manu_00
Contributor II

hey carlos,

thanks for your answer. Do you know if there are any documents  where i can find the information you provided to me? Or do i have to look in the header files to find out what functions are provided?

I changend the source code as you told me. But still no LED is blinking. I opened a serial port and i can see that the different tasks are created and executed once. As i understand the source code, the different tasks should be executd more than once. Can anybody help me.

Thanks in advance :-)

Manu

0 件の賞賛
返信