K60 RTC Vbat supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,255件の閲覧回数
marcosmarcoso
Contributor I

Hello,

we are using kinetis K60 (MK60DN512VLQ10). And we would like to use now an external battery to supply the RTC.

As we are working with VDD=1.8V, can the RTC work directly from a 3V battery?

In the datasheet K60P144M100SF2V2, I see that VBAT operating requirements are 1.71 to 3.6V, but I don't see any restriction respect VDD, is there any?

Thank you

best regards

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,839件の閲覧回数
EMontanez
NXP Employee
NXP Employee

Marcos,

K series products have separate VDD and VBAT domains. Both those domains support 1.71-3.6V supply ranges. The two domains can operate from independent supplies.

In summary, you can separate VBAT from VDD and operate it from a battery. :smileyhappy:

Best Regards,


Eduardo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,840件の閲覧回数
EMontanez
NXP Employee
NXP Employee

Marcos,

K series products have separate VDD and VBAT domains. Both those domains support 1.71-3.6V supply ranges. The two domains can operate from independent supplies.

In summary, you can separate VBAT from VDD and operate it from a battery. :smileyhappy:

Best Regards,


Eduardo

0 件の賞賛
返信