K60 I2C as slave.when I use function pointer, jump from main to boot, I2C SCL SDA from high change to low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 I2C as slave.when I use function pointer, jump from main to boot, I2C SCL SDA from high change to low

2,247件の閲覧回数
leimao
Contributor II

That's really strange. The master send cmd ask slave mcu,jump from main to boot, the slave mcu got right cmd, and when I use function pointer jump, The I2C

SCL and SDA will lock to low.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,044件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Lei,

I have checked TWR-K60N512 board, during the reset phase the I2C related pins are still keeping high voltage (with external pull-up resistor).

Could you provide the K60 I2C related circuit? And when the I2C slave get cmd to re-boot, during the slave in boot phase, what are master board doing? If the I2C related pin affected by master software?

Thank you for the attention.

0 件の賞賛
返信

2,044件の閲覧回数
leimao
Contributor II

Hi Hui:

     Thanks for youe help.

     I use scope to test I2C SDL and SCL. when rst, the master send nothing to slave.In face, when master send rst cmd, the master will silence 5 sec. when master start send cmd to slave, the slave allready in mainApp.

        And for I2C circuit, it works fine. The pull-up resistor we added in my pcb.

        I finally find a way to fix this problem. And I think this is a bug in kinetis. Before I jump from mainApp to Boot. I rst all interrupt, and rst scl SDA pin to orignal state. It finally works.    

0 件の賞賛
返信

2,044件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

If there exists bootloader similar application with slave MCU K60? If yes, it need to redirect the interrupt vector table for the application and the bootloader. Otherwise, it could cause interrupt service routine error.

Thank you for the attention.

0 件の賞賛
返信