K60 Flexbus Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 Flexbus Performance

6,267 Views
sithara
Contributor II

Since the internal RAM capacity is not sufficient, we plan to use external SRAM interfaced on flexbus.

What is the impact in performance when using external SRAM connected to flexbus instead of internal RAM ?

What is the Maximum Size of SRAM that can be connected to FlexBus?

Labels (1)
11 Replies

5,425 Views
juanandujar
Contributor I

Hello,

I am thinking to use the flexbus to connect a CPLD (16bits of register) with the microcontroller K60. I would like to know if it would be possible to use 16-bit data bus mode and address in multiplexed operating modes. It means, using the FB_AD[16:31] for data and address.

BR.

0 Kudos
Reply

5,425 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Juan,

It should be no problem for your case at all.


Hope that helps,

Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,425 Views
juanandujar
Contributor I

Hello,

I am reading the datasheet and I have found this:

• Address lines :      FB_AD from FB_AD0 upward

• Data lines

          • If CSCR[BLS] = 0, FB_AD from FB_AD31 downward

          • If CSCR[BLS] = 1, FB_AD from FB_AD0 upward

In my application I have a device with 16 bits of data and 16 bits of address. I want to use the FB_AD in this way:

Address:FB_AD[16:31]

Data:     FB_AD[16:31]

Would it be possible to set up in this way and how I should configure the registers  FB_CSPMCR ,FB_CSCRn and FB_CSMRn ?

BR.

0 Kudos
Reply

5,425 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Juan,

I think you have to use FB_AD[1:16] to connect with the address lines of the device, data connection should be fine, and for flexbus initialization, please kindly refer to the following sample code for details.

void TWRK60_flexbus_init(void){

/* Enable the FlexBus                                              */

/* Configure the FlexBus Registers for 8-bit port size              */

/*  with separate address and data using chip select 0              */

/* These configurations are specific to communicating with          */

/*  the MRAM used in this example                                  */

/* For K60 tower module - do not set byte lane shift so that data  */

/*  comes out on AD[31:24]                                          */

  //Set Base address

  FB_CSAR0 = (uint32)&MRAM_START_ADDRESS;

  FB_CSCR0  =  FB_CSCR_PS(1)      // 8-bit port

              | FB_CSCR_AA_MASK    // auto-acknowledge

              | FB_CSCR_ASET(0x1)  // assert chip select on second clock edge after address is asserted

              | FB_CSCR_WS(0x1)    // 1 wait state - may need a wait state depending on the bus speed

              ;

  FB_CSMR0  =  FB_CSMR_BAM(0x7)  //Set base address mask for 512K address space

              | FB_CSMR_V_MASK    //Enable cs signal

              ;

            

  //enable BE signals - note, not used in this example

  FB_CSPMCR = 0x02200000;

  //fb clock divider 3

  SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x3);

  /* Configure the pins needed to FlexBus Function (Alt 5) */

  /* this example uses low drive strength settings        */

  //address

  PORTB_PCR11 = PORT_PCR_MUX(5);          //  fb_ad[18]

  PORTB_PCR16 = PORT_PCR_MUX(5);          //  fb_ad[17]

  PORTB_PCR17 = PORT_PCR_MUX(5);          //  fb_ad[16]

  PORTB_PCR18 = PORT_PCR_MUX(5);          //  fb_ad[15]

  PORTC_PCR0  = PORT_PCR_MUX(5);          //  fb_ad[14]

  PORTC_PCR1  = PORT_PCR_MUX(5);          //  fb_ad[13]

  PORTC_PCR2  = PORT_PCR_MUX(5);          //  fb_ad[12]

  PORTC_PCR4  = PORT_PCR_MUX(5);          //  fb_ad[11]

  PORTC_PCR5  = PORT_PCR_MUX(5);          //  fb_ad[10]

  PORTC_PCR6  = PORT_PCR_MUX(5);          //  fb_ad[9]

  PORTC_PCR7  = PORT_PCR_MUX(5);          //  fb_ad[8]

  PORTC_PCR8  = PORT_PCR_MUX(5);          //  fb_ad[7]

  PORTC_PCR9  = PORT_PCR_MUX(5);          //  fb_ad[6]

  PORTC_PCR10 = PORT_PCR_MUX(5);          //  fb_ad[5]

  PORTD_PCR2  = PORT_PCR_MUX(5);          //  fb_ad[4]

  PORTD_PCR3  = PORT_PCR_MUX(5);          //  fb_ad[3]

  PORTD_PCR4  = PORT_PCR_MUX(5);          //  fb_ad[2]

  PORTD_PCR5  = PORT_PCR_MUX(5);          //  fb_ad[1]

  PORTD_PCR6  = PORT_PCR_MUX(5);          //  fb_ad[0]

  //data

  PORTB_PCR20 = PORT_PCR_MUX(5);          //  fb_ad[31] used as d[7]

  PORTB_PCR21 = PORT_PCR_MUX(5);          //  fb_ad[30] used as d[6]

  PORTB_PCR22 = PORT_PCR_MUX(5);          //  fb_ad[29] used as d[5]

  PORTB_PCR23 = PORT_PCR_MUX(5);          //  fb_ad[28] used as d[4]

  PORTC_PCR12 = PORT_PCR_MUX(5);          //  fb_ad[27] used as d[3]

  PORTC_PCR13 = PORT_PCR_MUX(5);          //  fb_ad[26] used as d[2]

  PORTC_PCR14 = PORT_PCR_MUX(5);          //  fb_ad[25] used as d[1]

  PORTC_PCR15 = PORT_PCR_MUX(5);          //  fb_ad[24] used as d[0]

  //control signals

  PORTB_PCR19 = PORT_PCR_MUX(5);          // fb_oe_b

  PORTC_PCR11 = PORT_PCR_MUX(5);          // fb_rw_b 

  PORTD_PCR1  = PORT_PCR_MUX(5);          // fb_cs0_b

  PORTD_PCR0  = PORT_PCR_MUX(5);          // fb_ale

}


Hope that helps,

Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,425 Views
juanandujar
Contributor I

Hello Kan_Li,

I know that the flexbus is able to work in the way you mention. However, my question is if it is possible to employ the upper bus for the address( FB_AD[16:31]). For instance, the data bus can be placed either in the lower or upper of the bus. With the address bus is possible to work in the same way.

0 Kudos
Reply

5,425 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Juan,

Actually I dont think it is possible to put address info on FB_AD[16:31] as this would exceed the address range mapping for flexbus , for example, if you want to access the data in 0xFFFF, you have to set the address pointer pointing to 0xFFFF0000 to drive 0xFFFF on FB_AD[16:31], but from RM, 0xA000_0000–0xDFFF_FFFF is the max mapping address range for flexbus. so that data info would not be driven on FB_AD[16:31] either.


Hope that helps,

Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,425 Views
Kan_Li
NXP TechSupport
NXP TechSupport

FlexBus timing is based on the FB_CLK signal, and it is 50MHz at max, while SRAM is based on the system clock, which is 100MHz or 120MHz depending on the part number, but if you select 120/150MHz part, which can enable cache for flexbus, so that would help to increase the performance. and there are 32 address lines available for this interface, but to enable the cache feature, the maximum size of SRAM can be 512MB. please kindly refer to the following for details.

1.png

Hope that helps,

B.R

Kan

5,425 Views
sithara
Contributor II


SRAM is asynchronous. Then what is the significance of FB_CLK?

0 Kudos
Reply

5,425 Views
Monica
Senior Contributor III

Hello Sithara,

have this worked for you? Please keep us posted, we'd like to know.

Best regards,

Monica

0 Kudos
Reply

5,425 Views
sithara
Contributor II

I have now planned to use DDR SDRAM interface and hence moved on to K61 processor with DDR interface.

5,425 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, I know external SRAM might be asynchronous, but the timing for signals of flexBus is based on FB_CLK, for example, the following figure shows the basic reading process of the flexBus.

1.png

so FB_CLK's frequency impacts the flexBus performance.

Please kindly let me know if you have any issue.

B.R

Kan