K60 FlexTimer (PWM) Example Code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 FlexTimer (PWM) Example Code?

Jump to solution
13,177 Views
nba916
Contributor I

I just downloaded example projects for the K60N512 TWR evaluation board, but there doesn't appear to be an example project for the FlexTimer module.  Does example code exist anywhere for download (preferably for CW)?

0 Kudos
Reply
1 Solution
3,949 Views
Charlie2000
Contributor I

After some struggle the following seems to work:

/*
 * pwm.c
 *
 *  Created on: 11 Nov 2011
 *      Author: Charles
 */
#include "derivative.h" /* include peripheral declarations */
#include "drivers.h"
#include "pwm.h"
#include "Clock.h"

#define FTM0_CLK_PRESCALE 1
#define FTM0_OVERFLOW_FREQUENCY (32000)

void InitPWM(void)
{
 
//Enable the Clock to the FTM0 Module
SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;  
 
//Pin control Register (MUX allowing user to route the desired signal to the pin.  
PORTC_PCR1   = PORT_PCR_MUX(0x4);  
PORTC_PCR2   = PORT_PCR_MUX(0x4);  
PORTC_PCR3   = PORT_PCR_MUX(0x4);  
PORTC_PCR4   = PORT_PCR_MUX(0x4);  
PORTD_PCR4   = PORT_PCR_MUX(0x4);  
PORTD_PCR5   = PORT_PCR_MUX(0x4);
 
//FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc.  
FTM0_MODE |= FTM_MODE_WPDIS_MASK;
 
//FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0
FTM0_MODE |= FTM_MODE_FTMEN_MASK;
 
//Set Edge Aligned PWM
FTM0_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;  
//QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled)
 
// Also need to setup the FTM0C0SC channel control register
FTM0_CNT = 0x0; //FTM Counter Value - reset counter to zero
FTM0_MOD = (PERIPHERAL_BUS_CLOCK/(1<<FTM0_CLK_PRESCALE))/FTM0_OVERFLOW_FREQUENCY ;  //Set the overflow rate
FTM0_CNTIN = 0; //Set the Counter Initial Value to 0
 
// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C0SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C0SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C0SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C1SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C1SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C1SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C2SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C2SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C2SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C3SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C3SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C3SC |= FTM_CnSC_MSB_MASK; //Channel Mode select
 
// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C4SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C4SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C4SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C5SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C5SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C5SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

//Edit registers when no clock is fed to timer so the MOD value, gets pushed in immediately
FTM0_SC = 0; //Make sure its Off!
 

//FTMx_CnV contains the captured FTM counter value, this value determines the pulse width
FTM0_C0V = FTM0_MOD/2;
FTM0_C1V = FTM0_MOD/2;
FTM0_C2V = FTM0_MOD/2;
FTM0_C3V = FTM0_MOD/2;
FTM0_C4V = FTM0_MOD/2;
FTM0_C5V = FTM0_MOD/2;
FTM0_COMBINE = FTM_COMBINE_COMBINE1_MASK;
FTM0_COMBINE = FTM_COMBINE_COMBINE0_MASK|FTM_COMBINE_COMP0_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN0_MASK|FTM_COMBINE_SYNCEN0_MASK|
               FTM_COMBINE_COMBINE1_MASK|FTM_COMBINE_COMP1_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN1_MASK|FTM_COMBINE_SYNCEN1_MASK|
               FTM_COMBINE_COMBINE2_MASK|FTM_COMBINE_COMP2_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN2_MASK|FTM_COMBINE_SYNCEN2_MASK;
 
FTM0_DEADTIME = FTM_DEADTIME_DTVAL(50); //About 5usec
/* SWOCTRL Bit Fields */
   //FTM0_SWOCTRL|= FTM_SWOCTRL_CH0OC_MASK|FTM_SWOCTRL_CH1OC_MASK|FTM_SWOCTRL_CH2OC_MASK|FTM_SWOCTRL_CH3OC_MASK|FTM_SWOCTRL_CH4OC_MASK|FTM_SWOCTRL_CH5OC_MASK;


//Status and Control bits
FTM0_SC =  FTM_SC_CLKS(1); // Selects Clock source to be "system clock" or (01)
//sets pre-scale value see details below
FTM0_SC |= FTM_SC_PS(FTM0_CLK_PRESCALE);
 
/******begin FTM_SC_PS details ****************************
* Sets the Prescale value for the Flex Timer Module which divides the
* Peripheral bus clock -> 48Mhz by the set amount
* Peripheral bus clock set up in clock.h
*  
* The value of the prescaler is selected by the PS[2:0] bits.  
* (FTMx_SC field bits 0-2 are Prescale bits -  set above in FTM_SC Setting)
*  
*  000 - 0 - No divide
*  001 - 1 - Divide by 2
*  010 - 2 - Divide by 4
*  011 - 3 - Divide by 8
*  100 - 4 - Divide by 16
*  101 - 5 - Divide by 32
*  110 - 6 - Divide by 64 -
*  111 - 7 - Divide by 128
*  ******end FTM_SC_PS details*****************************/
 
// Interrupts
//FTM0_SC |= FTM_SC_TOIE_MASK; //Enable the interrupt mask.  timer overflow interrupt.. enables interrupt signal to come out of the module itself...  (have to enable 2x, one in the peripheral and once in the NVIC
 
}

void UpdatePWM(unsigned short pwm1,unsigned short pwm2,unsigned short pwm3)
{
    unsigned mod = FTM0_MOD/2;
    FTM0_C0V = mod-pwm1;
    FTM0_C1V = mod+pwm1;
    FTM0_C2V = mod-pwm2;
    FTM0_C3V = mod+pwm2;
    FTM0_C4V = mod-pwm3;
    FTM0_C5V = mod+pwm3;
    FTM0_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK;
}


 

View solution in original post

0 Kudos
Reply
3 Replies
3,949 Views
Charlie2000
Contributor I

After some struggle the following seems to work:

/*
 * pwm.c
 *
 *  Created on: 11 Nov 2011
 *      Author: Charles
 */
#include "derivative.h" /* include peripheral declarations */
#include "drivers.h"
#include "pwm.h"
#include "Clock.h"

#define FTM0_CLK_PRESCALE 1
#define FTM0_OVERFLOW_FREQUENCY (32000)

void InitPWM(void)
{
 
//Enable the Clock to the FTM0 Module
SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;  
 
//Pin control Register (MUX allowing user to route the desired signal to the pin.  
PORTC_PCR1   = PORT_PCR_MUX(0x4);  
PORTC_PCR2   = PORT_PCR_MUX(0x4);  
PORTC_PCR3   = PORT_PCR_MUX(0x4);  
PORTC_PCR4   = PORT_PCR_MUX(0x4);  
PORTD_PCR4   = PORT_PCR_MUX(0x4);  
PORTD_PCR5   = PORT_PCR_MUX(0x4);
 
//FTM0_MODE[WPDIS] = 1; //Disable Write Protection - enables changes to QUADEN, DECAPEN, etc.  
FTM0_MODE |= FTM_MODE_WPDIS_MASK;
 
//FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0
FTM0_MODE |= FTM_MODE_FTMEN_MASK;
 
//Set Edge Aligned PWM
FTM0_QDCTRL &=~FTM_QDCTRL_QUADEN_MASK;  
//QUADEN is Bit 1, Set Quadrature Decoder Mode (QUADEN) Enable to 0,   (disabled)
 
// Also need to setup the FTM0C0SC channel control register
FTM0_CNT = 0x0; //FTM Counter Value - reset counter to zero
FTM0_MOD = (PERIPHERAL_BUS_CLOCK/(1<<FTM0_CLK_PRESCALE))/FTM0_OVERFLOW_FREQUENCY ;  //Set the overflow rate
FTM0_CNTIN = 0; //Set the Counter Initial Value to 0
 
// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C0SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C0SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C0SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C1SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C1SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C1SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C2SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C2SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C2SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C3SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C3SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C3SC |= FTM_CnSC_MSB_MASK; //Channel Mode select
 
// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C4SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C4SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C4SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

// FTMx_CnSC - contains the channel-interrupt status flag control bits
FTM0_C5SC |= FTM_CnSC_ELSB_MASK; //Edge or level select
FTM0_C5SC &= ~FTM_CnSC_ELSA_MASK; //Edge or level Select
FTM0_C5SC |= FTM_CnSC_MSB_MASK; //Channel Mode select

//Edit registers when no clock is fed to timer so the MOD value, gets pushed in immediately
FTM0_SC = 0; //Make sure its Off!
 

//FTMx_CnV contains the captured FTM counter value, this value determines the pulse width
FTM0_C0V = FTM0_MOD/2;
FTM0_C1V = FTM0_MOD/2;
FTM0_C2V = FTM0_MOD/2;
FTM0_C3V = FTM0_MOD/2;
FTM0_C4V = FTM0_MOD/2;
FTM0_C5V = FTM0_MOD/2;
FTM0_COMBINE = FTM_COMBINE_COMBINE1_MASK;
FTM0_COMBINE = FTM_COMBINE_COMBINE0_MASK|FTM_COMBINE_COMP0_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN0_MASK|FTM_COMBINE_SYNCEN0_MASK|
               FTM_COMBINE_COMBINE1_MASK|FTM_COMBINE_COMP1_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN1_MASK|FTM_COMBINE_SYNCEN1_MASK|
               FTM_COMBINE_COMBINE2_MASK|FTM_COMBINE_COMP2_MASK|/*FTM_COMBINE_DECAPEN0_MASK|FTM_COMBINE_DECAP0_MASK|*/
               FTM_COMBINE_DTEN2_MASK|FTM_COMBINE_SYNCEN2_MASK;
 
FTM0_DEADTIME = FTM_DEADTIME_DTVAL(50); //About 5usec
/* SWOCTRL Bit Fields */
   //FTM0_SWOCTRL|= FTM_SWOCTRL_CH0OC_MASK|FTM_SWOCTRL_CH1OC_MASK|FTM_SWOCTRL_CH2OC_MASK|FTM_SWOCTRL_CH3OC_MASK|FTM_SWOCTRL_CH4OC_MASK|FTM_SWOCTRL_CH5OC_MASK;


//Status and Control bits
FTM0_SC =  FTM_SC_CLKS(1); // Selects Clock source to be "system clock" or (01)
//sets pre-scale value see details below
FTM0_SC |= FTM_SC_PS(FTM0_CLK_PRESCALE);
 
/******begin FTM_SC_PS details ****************************
* Sets the Prescale value for the Flex Timer Module which divides the
* Peripheral bus clock -> 48Mhz by the set amount
* Peripheral bus clock set up in clock.h
*  
* The value of the prescaler is selected by the PS[2:0] bits.  
* (FTMx_SC field bits 0-2 are Prescale bits -  set above in FTM_SC Setting)
*  
*  000 - 0 - No divide
*  001 - 1 - Divide by 2
*  010 - 2 - Divide by 4
*  011 - 3 - Divide by 8
*  100 - 4 - Divide by 16
*  101 - 5 - Divide by 32
*  110 - 6 - Divide by 64 -
*  111 - 7 - Divide by 128
*  ******end FTM_SC_PS details*****************************/
 
// Interrupts
//FTM0_SC |= FTM_SC_TOIE_MASK; //Enable the interrupt mask.  timer overflow interrupt.. enables interrupt signal to come out of the module itself...  (have to enable 2x, one in the peripheral and once in the NVIC
 
}

void UpdatePWM(unsigned short pwm1,unsigned short pwm2,unsigned short pwm3)
{
    unsigned mod = FTM0_MOD/2;
    FTM0_C0V = mod-pwm1;
    FTM0_C1V = mod+pwm1;
    FTM0_C2V = mod-pwm2;
    FTM0_C3V = mod+pwm2;
    FTM0_C4V = mod-pwm3;
    FTM0_C5V = mod+pwm3;
    FTM0_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK;
}


 

0 Kudos
Reply
3,949 Views
mjg8t
Contributor IV

Thanks for the Code Charlie.  I was having a sorting through the registers based on needed functionality.  Your code was quite helpful.  

 

Note I did find 1 problem:

 

//FTMEN is bit 0, need to set to zero so DECAPEN can be set to 0
FTM0_MODE |= FTM_MODE_FTMEN_MASK;

 

Should be:

FTM0_MODE &=  ~FTM_MODE_FTMEN_MASK;

 

I was having problems updating my duty cycle and found that this was why.  

 

Cheers.

 


0 Kudos
Reply
3,949 Views
JJChiang
Contributor I

https://community.freescale.com/docs/DOC-1026

Message was edited by: JMc Updated link location.

0 Kudos
Reply