K60 FlexBus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,672件の閲覧回数
dporada
Contributor III

I'm trying to connect a 512k x 16bit sram chip to a TWR-K60D100M board using FlexBus.  To do this, I need 19 address bits, 16 data bits, CS, R/W, OE and ALE.  I am using a 74HC373 and latching A16, A17, and A18 with the ALE signal.

Here's the first question.  When I am addressing the memory at any location, the A30 (D14)  pin seems to be the same as the ALE signal.  If I disable the ALE signal, the A30 signal is still there so it's not a short.  I get this signal on the PRIMARY ELEVATOR board with only the TWR-K60D100M connected at pin B74.  Any Ideas?

The second question is about using a 16 bit bus.  When I try to write to an odd address, FlexBus writes to the odd and then the even address.  If I write to the even address, there is only one write.  Is this normal?

I tried looking at the TWR-MEM board since it uses a 16 bit memory chip, but it ties the upper and lower 8 bits together to make an 8 bit bus.

Thanks in advance for any help.

タグ(3)
0 件の賞賛
返信
1 解決策
2,430件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport


Hi

I check your attached code about Flexbus clock:
SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

Just remind: customer need to make sure the Flexbus clock not exceed 50MHz.

If you want to access TWR-MEM MRAM memory, the port size is 8-bit.

Customer can refer Kinetis 100MHz flexbus example code for more detailed info:

  FB_CSCR0  =   FB_CSCR_PS(1)      // 8-bit port

              | FB_CSCR_AA_MASK    // auto-acknowledge

              | FB_CSCR_ASET(0x1)  // assert chip select on second clock edge after address is asserted

              | FB_CSCR_WS(0x1)    // 1 wait state - may need a wait state depending on the bus speed

              ;

Wish it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,430件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Donald,

1> About TWR-K60D100M PTB21 pin status, customer need to check if set PORTB_PCR21 register [MUX] bits with ALT5 function.
I checked K60 100MHz Flexbus module validation report, there is no record info about Flexbus pin function with problem.

2> That performance is caused by Flexbus address misaligned transfer.

Thank you for the attention.

0 件の賞賛
返信
2,430件の閲覧回数
dporada
Contributor III

Here's the code.  Most was copied from the app notes.

 

  PORTC_PCR3 = (PORTC_PCR3 & ~PORT_PCR_DSE_MASK) | PORT_PCR_DSE(1) ;

 

  SIM_SCGC7 |= SIM_SCGC7_FLEXBUS_MASK; // Enable the clock to the FlexBus

  SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

  // Set the GPIO ports clocks

  SIM_SCGC5 = SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK |

  SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK;

 

  PORTB_PCR20 = PORT_PCR_MUX(5);  //  fb_ad[31] used as d[15]

  PORTB_PCR21 = PORT_PCR_MUX(5);  //  fb_ad[30] used as d[14]

  PORTB_PCR22 = PORT_PCR_MUX(5);  //  fb_ad[29] used as d[13]

  PORTB_PCR23 = PORT_PCR_MUX(5);  //  fb_ad[28] used as d[12]

  PORTC_PCR12 = PORT_PCR_MUX(5);  //  fb_ad[27] used as d[11]

  PORTC_PCR13 = PORT_PCR_MUX(5);  //  fb_ad[26] used as d[10]

  PORTC_PCR14 = PORT_PCR_MUX(5);  //  fb_ad[25] used as d[9]

  PORTC_PCR15 = PORT_PCR_MUX(5);  //  fb_ad[24] used as d[8]

  PORTB_PCR6  = PORT_PCR_MUX(5);  //  fb_ad[23] used as d[7]

  PORTB_PCR7  = PORT_PCR_MUX(5);  //  fb_ad[22] used as d[6]

  PORTB_PCR8  = PORT_PCR_MUX(5);  //  fb_ad[21] used as d[5]

  PORTB_PCR9  = PORT_PCR_MUX(5);  //  fb_ad[20] used as d[4]

  PORTB_PCR10 = PORT_PCR_MUX(5);  //  fb_ad[19] used as d[3]

  PORTB_PCR11 = PORT_PCR_MUX(5);  //  fb_ad[18] used as d[2]

  PORTB_PCR16 = PORT_PCR_MUX(5);  //  fb_ad[17] used as d[1]

  PORTB_PCR17 = PORT_PCR_MUX(5);  //  fb_ad[16] used as d[0]

  PORTB_PCR18 = PORT_PCR_MUX(5);  //  fb_ad[15]

  PORTC_PCR0  = PORT_PCR_MUX(5);  //  fb_ad[14]

  PORTC_PCR1  = PORT_PCR_MUX(5);  //  fb_ad[13]

  PORTC_PCR2  = PORT_PCR_MUX(5);  //  fb_ad[12]

  PORTC_PCR4  = PORT_PCR_MUX(5);  //  fb_ad[11]

  PORTC_PCR5  = PORT_PCR_MUX(5);  //  fb_ad[10]

  PORTC_PCR6  = PORT_PCR_MUX(5);  //  fb_ad[9]

  PORTC_PCR7  = PORT_PCR_MUX(5);  //  fb_ad[8]

  PORTC_PCR8  = PORT_PCR_MUX(5);  //  fb_ad[7]

  PORTC_PCR9  = PORT_PCR_MUX(5);  //  fb_ad[6]

  PORTC_PCR10 = PORT_PCR_MUX(5);  //  fb_ad[5]

  PORTD_PCR2  = PORT_PCR_MUX(5);  //  fb_ad[4]

  PORTD_PCR3  = PORT_PCR_MUX(5);  //  fb_ad[3]

  PORTD_PCR4  = PORT_PCR_MUX(5);  //  fb_ad[2]

  PORTD_PCR5  = PORT_PCR_MUX(5);  //  fb_ad[1]

  PORTD_PCR6  = PORT_PCR_MUX(5);  //  fb_ad[0]

 

 

 

  PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b

  PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b

  PORTD_PCR1  = PORT_PCR_MUX(5); // fb_cs0_b

  PORTD_PCR0  = PORT_PCR_MUX(5); // fb_ale

 

  PORTC_PCR3  = PORT_PCR_MUX(5); // fb_clk

  FB_CSCR0  =   FB_CSCR_PS(0x02)      // 16-bit port

              | FB_CSCR_AA_MASK    // auto-acknowledge

                  | FB_CSCR_WS(0x2)    // 2 wait states

              ;

 

  FB_CSMR0 = FB_CSMR_BAM(0xF)  //Set base address mask for 1M address space

             | FB_CSMR_V_MASK    //Enable cs valid signal

             ;

 

 

  FB_CSAR0 = (0x60000000); //Set Base address 

  

0 件の賞賛
返信
2,431件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport


Hi

I check your attached code about Flexbus clock:
SIM_CLKDIV1 |= SIM_CLKDIV1_OUTDIV3(0x0); //FlexBus Clock not divided

Just remind: customer need to make sure the Flexbus clock not exceed 50MHz.

If you want to access TWR-MEM MRAM memory, the port size is 8-bit.

Customer can refer Kinetis 100MHz flexbus example code for more detailed info:

  FB_CSCR0  =   FB_CSCR_PS(1)      // 8-bit port

              | FB_CSCR_AA_MASK    // auto-acknowledge

              | FB_CSCR_ASET(0x1)  // assert chip select on second clock edge after address is asserted

              | FB_CSCR_WS(0x1)    // 1 wait state - may need a wait state depending on the bus speed

              ;

Wish it helps.

0 件の賞賛
返信