K60: External clock characteristics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60: External clock characteristics

ソリューションへジャンプ
3,040件の閲覧回数
mike65535
Contributor II

I'm trying to find a spec for the electrical requirements for providing an external clock to the K60.

I currently have a circuit that puts a sinewave on "EXTAL", a sinewave that has a DC component of about 0.8V and a pk-to-pk voltage of about 0.7V

I get intermittent hanging at this in bsp_cm

while ((MCG_S & MCG_S_IREFST_MASK) != 0x00U)  /* Check that the source of the FLL reference clock is the external reference clock. */

{

}

making me suspicious of the clock.

タグ(4)
0 件の賞賛
返信
1 解決策
2,534件の閲覧回数
apanecatl
Senior Contributor II

Hi Mike, here are the XTAL pin electrical specifications, depending on the oscillator mode (low power or high gain) the signal amplitude can be either .6V or VDD, the full table can be found in chapter 6.3.2 Oscillator electrical characteristics of the K60 datasheet:

2817_2817.png

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,534件の閲覧回数
JimDon
Senior Contributor III
0 件の賞賛
返信
2,534件の閲覧回数
mike65535
Contributor II

I've seen that and it doesn't tell me what I need to know.

I'd like to know the peak-to-peak amplitude and the DC offset it can tolerate of an external clock signal provide on EXTAL.

For ex, must the clock go from, say 0.5V to 1.5 V, or say from 0.8V to 1.8V or what?

0 件の賞賛
返信
2,535件の閲覧回数
apanecatl
Senior Contributor II

Hi Mike, here are the XTAL pin electrical specifications, depending on the oscillator mode (low power or high gain) the signal amplitude can be either .6V or VDD, the full table can be found in chapter 6.3.2 Oscillator electrical characteristics of the K60 datasheet:

2817_2817.png

0 件の賞賛
返信