K60-100MHz UART Receive with Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60-100MHz UART Receive with Interrupt

1,410件の閲覧回数
pallenna
Contributor II

Dear Friends,

I have tried the data receive from Serial port with UART  in polling mode it is working fine but when i am trying with Interrupt it is going to default ISR please suggest me and if any body have example code please post here. And i am posting the code what am using please correct me any mistakes are there.I am asking this for K60 with 100MHz Tower. I have already tried this with K60-120 there it is working fine and am facing problem with K60-100 Board. Please suggest me.

 

 

Thanks & Regards,

Padmaja.P

Original Attachment has been moved to: uart.c.txt.zip

Original Attachment has been moved to: isr.h.txt.zip

タグ(2)
0 件の賞賛
返信
1 返信

1,081件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

I already answered to you in the thread:

UART transmition in isr for k60

it is a similar question.


Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信