K40 FOR IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K40 FOR IAR

1,638件の閲覧回数
WayneChung
Contributor I

I use the IAR ARM sample example,

 

when i set "GPIOC_PSOR = 1" ,

 

the Register will set to "GPIOC_PDORC = 1" .

 

0 件の賞賛
返信
1 返信

1,464件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

This sounds to be normal operation. GPIOC_PSOR is the Set Output Register, causing the bit with '1' to be set to the output; the register itself always reads 0.

Since the write set the bit in the output, this is seen in the GPIOC_PDORC register.

 

By contrast, if you write "GPIOC_PCOR = 1" it will then clear the bit in the GPIOC_PDORC register.

Furthermore "GPIOC_PTOR = 1" will toggle the bit.

 

 

Regards

 

Mark

 

0 件の賞賛
返信