K32 L2A Force RESETn pin to be dedicated

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K32 L2A Force RESETn pin to be dedicated

跳至解决方案
2,365 次查看
sachin_patel
Contributor IV

Hi,

 

I am using a Kinetis K32 L2A microcontroller in our design. As part of our model, we require the RESETn pin to be dedicated (i.e. it must not be possible from software to change it's pin mux state).

I can see in the Reference Manual Chapter 6.3.2: FTFA_FOPT[3]:

RESET_PIN_CFG: When set to 1, it says the following: "RESET_b pin is dedicated. The port is configured with pullup enabled, open drain, passive filter enabled".

Does this mean that the option to mux the pin as anything other than RESET_b is now disabled?

Thanks,

Sachin Patel

0 项奖励
回复
1 解答
2,354 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,355 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

0 项奖励
回复