K28F COLORBURST

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K28F COLORBURST

2,025件の閲覧回数
javierhernande1
Contributor IV

Hello,

I', using a Video Sync Separator with the K28F to get the luminance to text/graphic overlay, connecting it to the analog comparator module.

Also, I would to get the chrominance, in order to change the color text/graphics. I have seen that with a microcontroller it's possible using a crystal oscillator of 14.3181 MHz. I'm using a external 32.768Khz crystal in my project.

I could to use someone the internal clocks of the K28F to it? or I will need to add a external crystal?

Best regards

Arduino TVoutColor NTSC - YouTube 

ラベル(1)
3 返答(返信)

1,870件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I am not quite sure if I understand you correctly. If not, please correct me.

For your application, I do think an internal clock can been used without problems. From the manual, you can see below:

pastedImage_1.png

So both OSCERCLK and IRC48MCLK internal clock can been used as adc module.

1,870件の閲覧回数
javierhernande1
Contributor IV

Hello Fang Li,

Thanks for the reply,

I'm reading this but I haven't finished yet.

You want to say that I can adjust OSCERCLK or IRC48MCLK to 14.3181 Mhz via software?

Best regards

0 件の賞賛
返信

1,870件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Javier

yes, you can config an external clock for ADC by select ALTCLK (ADCx_CFG1[ADICLK] = 10) and input an external clock to EXTAL/XTAL pins. ALTCLK is connected to OSCERCLK.