K28 Vrefh pin connection option

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K28 Vrefh pin connection option

1,465 次查看
jasonlarson
Contributor II

I have a design that is power sensitive put I also need accurate adc readings. For this reason I'm adding a external prec ref voltage source. I will not be doing measurements all the time and If I shut down the prec ref I can save about 100ua. The only issue is that the Vrefh pin into the micro will be floating. Will this be a issue? The data sheet says unused pins short go to VDD but what happens if I let it float? Since I will not be doing any reading I would think it should not be a issue. It will have a impedance to gnd through the prec ref chip. Would that be good or bad?

0 项奖励
回复
1 回复

1,361 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi Jason,

I think it is ok if it float to ground. Please see  this link:

https://community.nxp.com/message/419427?commentID=419427#comment-419427

Regards,

Jing