K26 Overshoot acceptance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K26 Overshoot acceptance

1,067 Views
pradeeppatil
Contributor I

I am running Signal integrity simulation using K26 IBIS model and SDram device, but i am able to see overshoot at K26 for read condition So anybody tell me What is maximum overshoot acceptance for K26 device ?

1 Reply

1,008 Views
michael_galda
NXP Employee
NXP Employee

Do you mean the voltage overshoot acceptance on the MCU input pins?

This is VDD+0.3V / VSS-0.3V

So if the VDD = 3.3V

Then the input signals should be in range -0.3V to 3.6V