K24 RTC compenstation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K24 RTC compenstation

跳至解决方案
3,289 次查看
yuanli
NXP Employee
NXP Employee

Hi,

Is there any doc to guidance how to compensate K24 RTC?

Customer is using external RTC clock, When run the MCU continuously for 5 days, there are 23 seconds difference between MCU and PC.

Please help advise how to compensate it, thanks.

Best regards,

Ryan

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,050 次查看
santiago_gonzal
NXP Employee
NXP Employee
3 回复数
3,050 次查看
egoodii
Senior Contributor III

You should be able to do 'a lot better' than 4s/day just by setting the proper chip load-capacitors.  See my discussion:

Re: RTC accuracy with MQX 4.1 on a K70

But as I say there, your 'worst case parts' will still only get you about 2s/day at room temperature with 'inexpensive' crystals -- a nice oscillator can hold 1s/day.  The APNOTE mentioned above helps you improve a crystal over temperature, BUT that requires the CPU to be 'awake', at least periodically, to be able to MEASURE said temperature and 'do something with it' -- the SiTime part 'does that for you'.

3,050 次查看
yuanli
NXP Employee
NXP Employee

Thanks a lot for the advices from both of you, I will study and have a try. :smileyhappy:

0 项奖励
回复
3,051 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello Yuan Li,

Have a look here:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4949.pdf

Regards,

Santiago