K22F Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22F Bootloader

1,548件の閲覧回数
elinaiman
Contributor I

Hi
I am wondering if you can help me. I am using the KDS based on Eclipse to develop my application. I have a FRDM-K22F board which the KDS can not communicate with. I understand that the procedure is to put the board in BOOTLOADER mode and then drag-and-drop a file to it.
My question is which file:
DEBUG-FRDM-K22F-Pemicro_v108b_for_open_SDA_v2.1.bin
OR
MSD-DEBUG-FRDM-K22F_Pemicro_v114.SDA

Thanks for your help

タグ(1)
0 件の賞賛
返信
1 返信

1,444件の閲覧回数
BlackNight
NXP Employee
NXP Employee

See the following thread: https://community.nxp.com/message/946384 

0 件の賞賛
返信