K22F + 32 Khz Xtal + FLL + USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22F + 32 Khz Xtal + FLL + USB

ソリューションへジャンプ
1,759件の閲覧回数
chriskeeser
Contributor III

Is it acceptable to run the USB module from the FLL if the source for the FLL is the external 32 Khz xtal?  I have had a difficult time finding concrete information that says this is ok or not.

I did stumble across this site µTasker MCG Configuration Support  that seemed to indicate the FLL was not suitable for USB operation.

"Note that the output from the FLL has higher jitter than that from the PLL and is not suitable as clock source for USB. For USB host mode, only the PLL should be used to derive its 48MHz clock from unless a dedicated USB clock signal is available. The same is true for USB device unless the Kinetis part includes IRC48M, which can be used to fulfil USB device specification requirements."

Any help here would be appreciated.

Note the FLL output is 96 Mhz.

0 件の賞賛
返信
1 解決策
1,611件の閲覧回数
mjbcswitzerland
Specialist V

Chris

All user manuals have this, which warns about using the FLL output since it doesn't meet USB certification requirements.

pastedImage_1.png

For serious work the FLL should not be considered as a possible source.

Regards

Mark

元の投稿で解決策を見る

2 返答(返信)
1,612件の閲覧回数
mjbcswitzerland
Specialist V

Chris

All user manuals have this, which warns about using the FLL output since it doesn't meet USB certification requirements.

pastedImage_1.png

For serious work the FLL should not be considered as a possible source.

Regards

Mark

1,611件の閲覧回数
chriskeeser
Contributor III

Thank you for your concise response.

0 件の賞賛
返信