K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?

1,676 Views
sharadpatil
Contributor I

Hi,

I am working on UART communication module of MK22FX512VMC12 controller. K22 controller operated on 3.3V supply and external communication module operated on 5V supply.my communication is working properly with external module.

As per datasheet gpio pins operated on 5V  but no idea about uart communication module operating pin voltage 5V.

Is it ok if i connect K22 controller UART pins(Txd, Rxd) to 5V operated module(Txd ,Rxd pins) ?

pastedImage_3.png

Thanks,

#Sharad‌

Tags (2)
0 Kudos
Reply
1 Reply

1,438 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sharad,

The Kinetis Port pins are only 5V tolerant as inputs.  The outputs are not 5V tolerant, and that includes pins configured as open-drain outputs(Don't pullup to 5V).

Output pins(TXD) would only be driven to 3.3V. If the 5V device will recognize that as a high, then it's ok.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply