K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22 controller pin(TXD and RXD uart pins) operated on 5V (external device working on 5V supply)?

1,670件の閲覧回数
sharadpatil
Contributor I

Hi,

I am working on UART communication module of MK22FX512VMC12 controller. K22 controller operated on 3.3V supply and external communication module operated on 5V supply.my communication is working properly with external module.

As per datasheet gpio pins operated on 5V  but no idea about uart communication module operating pin voltage 5V.

Is it ok if i connect K22 controller UART pins(Txd, Rxd) to 5V operated module(Txd ,Rxd pins) ?

pastedImage_3.png

Thanks,

#Sharad

タグ(2)
0 件の賞賛
返信
1 返信

1,432件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Sharad,

The Kinetis Port pins are only 5V tolerant as inputs.  The outputs are not 5V tolerant, and that includes pins configured as open-drain outputs(Don't pullup to 5V).

Output pins(TXD) would only be driven to 3.3V. If the 5V device will recognize that as a high, then it's ok.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信