K22(MK22FN512CAP12R) using ISO 7816

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22(MK22FN512CAP12R) using ISO 7816

1,493 Views
yaochiayang
Contributor I

Hi all,

for ISO7816, three pins are used for communication.

CLK, I/O and RST.

I/O

I will connect I/O with UART0_TX, for I could see in some document UART_TX could be configured to I/O pin for 7816 standard.

also, UART0 are the only one which supports ISO7816 in K22 120MHz.

RST

i will connect RST to UART0_RTS_b.

CLK

i see this information in the forum as well. CLK is suggested to tie with FTM.

i am gonna connect this with FTM0_CH5. is this feasible?

as far as i learn from the reference manual, it seems configurable though.

is the way connection gonna work for SW?

thanks,

Lawrence

Labels (1)
0 Kudos
Reply
1 Reply

1,107 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Lawrence,

I am sorry, but the ISO7816 RST signal is a reset signal, not the function of UART RTS(Request to send), so if you connected RST to UART0_RTS_b, you should configure this pin as GPIO function, not the UART0_RTS_b function.

Hope that helps,


Have a great day,
Kan

Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply