K22 ADC Calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22 ADC Calibration

1,546 Views
sbranover
Contributor I

When non volatile memory is available is it recommended to store and reload the ADC calibration values or is it better to run the auto calibration at every reboot?

We are also storing calibration values for circuitry external to the ADC for which the calibration needs to be preformed in a lab.

Labels (1)
0 Kudos
Reply
1 Reply

1,445 Views
nxf56274
NXP Employee
NXP Employee

Hi,

pastedImage_1.png

You would better run the auto calibration at every reboot. Because some factors ,such as temperature, will influence the  the calibration value. So the fixed value will influence the ADC's preciseness.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply