K21 serial MCU JTAG Instruction

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K21 serial MCU JTAG Instruction

Jump to solution
3,199 Views
張峻瑞
Contributor I

Question,

1. MK21FN1M0VMC12 and MK21FN1M0VLQ12 JTAG Instruction is the same?

2. The PDF(K21 Sub-Family Reference Manual) JTAG section equal MK21FN1M0VMC12 and MK21FN1M0VLQ12 JTAG Instruction?

K21 Sub-Family Reference Manual

Supports: MK21DX128VLK5, MK21DX256VLK5, MK21DN512 VLK5

http://cache.freescale.com/files/32bit/doc/ref_manual/K21P80M50SF4RM.pdf

I can download to MK21FN1M0VMC12 , but I can`t download to MK21FN1M0VLQ12 .... (Use TWR-K21F120M Tower Module)

I think maybe is JTAG Instruction not equal...:smileyconfused:

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,891 Views
Rick_Li
NXP Employee
NXP Employee

Hi,

the JTAG instructions set is same for MK21FN1M0VMC12 and MK21FN1M0VLQ12.

I dont exactly know what is the problem on your side, are you using a J-Link to program the device?

or are you using the OS-JTAG debugger integrated on the board to program the MCU, if so, then, how do you change the MCU on the board?

please give me more description!

View solution in original post

0 Kudos
Reply
4 Replies
2,892 Views
Rick_Li
NXP Employee
NXP Employee

Hi,

the JTAG instructions set is same for MK21FN1M0VMC12 and MK21FN1M0VLQ12.

I dont exactly know what is the problem on your side, are you using a J-Link to program the device?

or are you using the OS-JTAG debugger integrated on the board to program the MCU, if so, then, how do you change the MCU on the board?

please give me more description!

0 Kudos
Reply
2,891 Views
張峻瑞
Contributor I

Hi, Li:

I using the OSJTAG download to MCU, the development board is TWR-K21F120M Tower Module

detail process:

1. OPEN TWR-K21F120M - J8 let MCU(MK21FN1M0VMC12 ) no power.

2. Connect J1(JTAG) to my design board (MCU: MK21FN1M0VLQ12), there is pin to pin.

3.  Connect microUSB cable to J2  and power on.

4. CodeWarrior 10.6 download to my design board.

5. fail, find OSJTAG but not find MCU(MK21FN1M0VLQ12).

Only TWR-K21F120M downloaf is OK.

Thanks.

0 Kudos
Reply
2,891 Views
Rick_Li
NXP Employee
NXP Employee
0 Kudos
Reply
2,891 Views
張峻瑞
Contributor I

Yes, Thank you very much.

0 Kudos
Reply