K21 Tamper question from AN4733

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K21 Tamper question from AN4733

2,058 Views
PHXFAE
Contributor II

Looking at AN4733 figure 1, it looks like the Tamper inputs are in the VBAT power domain but I don’t see a path to clear the key.  It doesn’t look like the tamper
pins can erase the key.  Are these pins only useful if main power is on?

Labels (1)
0 Kudos
Reply
2 Replies

1,789 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

I just got the feedback, the expert told me there is some issue for Figure 1, which is not complete/accurate, but she assured me that the tamper inputs are connected to the key erase logic.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,789 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Alex,

I am checking with the DryIce expert, and will let you known when I have any more information.

Thanks for your patience!


Have a great day,
Kan

0 Kudos
Reply