K21 - DryIce data loss, high VBAT current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K21 - DryIce data loss, high VBAT current

3,977件の閲覧回数
michaelhaben
Contributor I

We're using the DryIce tamper module in a K21, and seeing unexplained loss of stored data even with all tamper-sources disabled.

Our suspicion was that the VBAT line was somehow glitching below the DryIce minimum limit of 1.71V, despite having a 1kohm/1uF RC filter on it - in the course of investigation, we've seen up to 28uA being drawn by the K21 VBAT line (28mV across the 1k resistor) when the main power-supply is switched off, way above any figure given in the datasheet!  So please can anyone tell me...

1.  Does VBAT supply any K21 modules other than DryIce and the RTC?

2.  What could be causing such a high current to be drawn?

3.  Is anyone using the K21 DryIce tamper module successfully and reliably?  Any tips to share?

thanks,  Mike

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

3,715件の閲覧回数
michaelhaben
Contributor I

Hi Fang,

  we are definitely seeing ~30uA being drawn by the VBAT pin, but only from abot 2 seconds after power-up, indicating that we might be configuring the DryIce wrongly.  I can't find any information in the datasheet on the drive-strength (output current) of the tamper-pins, please can you tell me where to find this info?

thank you,  Mike H.

0 件の賞賛
返信

3,715件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Answer to your questions:

1. Yes, VBAT is independent power supply for DryIce and RTC, no others.

2. It is really hard to give more detail information regarding this. The Drylce more detail information need an NDA.

0 件の賞賛
返信

3,715件の閲覧回数
michaelhaben
Contributor I

Thank you for confirming that Vbat supplies only RTC and DryIce. We signed

an NDA at the start of the project, and have the DryIce example code etc.

0 件の賞賛
返信

3,715件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Michael

I see that you had submit a case regarding this issue. I will help you on this regard. Would you mind sent me the schematic? I would like to check the hardware connection first, especially the connect of VBAT and main VDD.

0 件の賞賛
返信

3,715件の閲覧回数
michaelhaben
Contributor I

Hi Fang, I hope you can see this - 

I tried to reply to your email, but received the response below.  Do you have a personal email address I can send the schematic to?

Thank you,  Mike H.

Dear Customer,

We assume that your email was intended to receive support from NXP technical support.

Due to legal reasons we are not allowed to interact with unidentified contacts.

 

Therefore, please connect to http://www.nxp.com/support for further assistance. You may

have to login and/or register before submitting a case.

 

If your email was in reply to an active or recently closed support case, please make sure

that the original email subject you received from NXP is used in the email you send  to

enable automatic routing. 

 

Please adjust and re-send your message to [email protected].

 

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

 

 

Best Regards,

Technical Support

NXP Semiconductor

 

The information contained in this email is classified as:

[X] Public Information

0 件の賞賛
返信

3,715件の閲覧回数
michaelhaben
Contributor I

Further measurements on a different board: once the DryIce has been configured, with the main MCU power OFF, I am seeing a steady 19uA being drawn by the VBAT pin.  With MCU power ON, the VBAT current is higher, typically 32 - 40uA but sometimes up to 70-80uA!

0 件の賞賛
返信

3,715件の閲覧回数
michaelhaben
Contributor I

Hi Fang, please can you tell me how to send the schematic of our circuit

to you?  I'd rather not post it on a public forum!

thanks,  Mike

0 件の賞賛
返信