K20DX JTAG Pull-up/down

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K20DX JTAG Pull-up/down

Jump to solution
4,580 Views
luc_meijer
Contributor I

Hi

In my current design I'm using the MK20DX256VLH7 MCU. I would like to add a JTAG connector but are not sure if I need to add external Pull-up/down resistors. The reference manual states that they are Internal.

Does this mean that there are no external Pull-up/down resistors are necessary?

pastedImage_1.png

Best regards,

Luc

Labels (1)
0 Kudos
Reply
1 Solution
4,471 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Luc Meijer

We recommend adding an external strong pull-up resistor (typically of 10k ohm ) on the  JTAG_TMS pin.  

Here you can see a reference in the KQRUG (attached bellow ). on page 33. 

JTAG.PNG

Also, I believe that this post can be useful    Design Considerations for Debug

Alternatively, you could check the JTAG interface in the schematic of our Freedom boards. 

If I can help you further, please let me know.

 Best regards, Diego.

 ------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
4,472 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello, Luc Meijer

We recommend adding an external strong pull-up resistor (typically of 10k ohm ) on the  JTAG_TMS pin.  

Here you can see a reference in the KQRUG (attached bellow ). on page 33. 

JTAG.PNG

Also, I believe that this post can be useful    Design Considerations for Debug

Alternatively, you could check the JTAG interface in the schematic of our Freedom boards. 

If I can help you further, please let me know.

 Best regards, Diego.

 ------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply